LPC1317 peripheral on almost any pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1317 peripheral on almost any pins

Jump to solution
3,062 Views
MJ1
Contributor I

Hi

Is possible to reconnect/repin peripherals on LPC1317 HVQFN33 package to pins which are not intended in manual for that peripheral? I.e. UART/USART RXD, TDX signals to SPI MOSI, MISO - PIO0_21, PIO0_22 pins?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
3,053 Views
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

View solution in original post

0 Kudos
Reply
2 Replies
3,054 Views
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

0 Kudos
Reply
3,051 Views
MJ1
Contributor I

Thanks so much.

0 Kudos
Reply