LPC1313 SSP0 bit rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1313 SSP0 bit rate

ソリューションへジャンプ
3,848件の閲覧回数
prachipanse
Contributor III

Hi,

I am trying to set the bit rate of the SSP0 port of the LPC1313FBD48/01 to 1MHz. The system clock is 72MHz, and it is divided by 12 to have the SSP clock as 6MHz. I have checked the CPSDVSR = 2 and SCR = 2, which should give me 1MHz:

Bit frequency = Pclk/(CPSDVSR * (SCR + 1))

However, I get 781.2kHz in place of 1MHz. 

What might be going wrong here?

Regards,

Prachi

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
3,608件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi prachi panse,

Thanks for your reply.

If the system clock is located in the range of 71 to 72 MHz, the observed frequency: 992kHz can be considered correct according to below formula.

Bit frequency = Pclk/(CPSDVSR * (SCR + 1))

Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,608件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi prachi panse,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

I was wondering if you can share the screenshot of values of the corresponding registers under debugging.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,608件の閲覧回数
prachipanse
Contributor III

Hi,

I have tested with the same settings on another board and see that the bit clock gets set to 992kHz instead of 1MHz. The SSP0 registers are as below:

pastedImage_1.png

Please let me know if these values are as expected to achieve 1MHz bit rate.

Thanks and Regards,

Prachi

0 件の賞賛
返信
3,608件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi prachi panse,

Thank for your reply.

It's so weird, to dig the more deeper, can you share the wave of system clock via clkout pin?
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,608件の閲覧回数
prachipanse
Contributor III

Thanks. I have observed the system clock on the CLKOUT pin and it comes to be around 71-72MHz.

0 件の賞賛
返信
3,609件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi prachi panse,

Thanks for your reply.

If the system clock is located in the range of 71 to 72 MHz, the observed frequency: 992kHz can be considered correct according to below formula.

Bit frequency = Pclk/(CPSDVSR * (SCR + 1))

Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信