LPC11U68 RTC configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U68 RTC configuration

2,956 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Mon Sep 08 13:24:47 MST 2014
Hi,

For the first time I'm using an LPC11U68 microprocessor.
It's not clear for me if, in order to obtain an Real Time Clock, some external components are necessary (crystal and capacitors at pins RTCXIN and RTCXOUT) or the microprocessor has a complete internal generato for this purpose.
Can anybody help me?

Thanks in advance!

Mattia
Labels (1)
0 Kudos
Reply
6 Replies

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dariush_abbasi868 on Mon Jun 29 01:12:23 MST 2015
Hi,
In LPCOPEN sample code there isn't any clear sample to read hour and minute and ... for lpc11e68 .
Is it has  LPC_RTC->SEC or somthing like that ?
0 Kudos
Reply

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Fri Sep 12 14:45:17 MST 2014
Hi,

Please also refer to the "RTC oscillator component selection" in the datasheet to select the correct capacitors for the 32 kHz crystal you will be using.

Thanks.

nxp support
0 Kudos
Reply

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Tue Sep 09 12:03:33 MST 2014
Thank you very much!
Question Solved
0 Kudos
Reply

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 08 14:44:22 MST 2014
Yes, as described in Datasheet and UM10732:


Quote:
8.22 Real-Time Clock (RTC)
The RTC resides in a separate always-on voltage domain with battery back-up. The RTC uses an[color=#f00] independent oscillator[/color], also located in the always-on voltage domain.


0 Kudos
Reply

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Mon Sep 08 14:22:01 MST 2014
Thank you,

so you can confirm me that the crystal is necessary? This is what I suppose.
0 Kudos
Reply

2,642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 08 13:39:05 MST 2014
Hardware: RTC Hardware is described in schematic of LPCXpresso LPC11U68:

http://www.embeddedartists.com/products/lpcxpresso/lpc11U68_xpr.php

Software: LPCOpen should include a RTC sample:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0
0 Kudos
Reply