LPC11U68 RTC configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11U68 RTC configuration

2,968 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Mon Sep 08 13:24:47 MST 2014
Hi,

For the first time I'm using an LPC11U68 microprocessor.
It's not clear for me if, in order to obtain an Real Time Clock, some external components are necessary (crystal and capacitors at pins RTCXIN and RTCXOUT) or the microprocessor has a complete internal generato for this purpose.
Can anybody help me?

Thanks in advance!

Mattia
标签 (1)
0 项奖励
回复
6 回复数

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dariush_abbasi868 on Mon Jun 29 01:12:23 MST 2015
Hi,
In LPCOPEN sample code there isn't any clear sample to read hour and minute and ... for lpc11e68 .
Is it has  LPC_RTC->SEC or somthing like that ?
0 项奖励
回复

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp_apps on Fri Sep 12 14:45:17 MST 2014
Hi,

Please also refer to the "RTC oscillator component selection" in the datasheet to select the correct capacitors for the 32 kHz crystal you will be using.

Thanks.

nxp support
0 项奖励
回复

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Tue Sep 09 12:03:33 MST 2014
Thank you very much!
Question Solved
0 项奖励
回复

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 08 14:44:22 MST 2014
Yes, as described in Datasheet and UM10732:


Quote:
8.22 Real-Time Clock (RTC)
The RTC resides in a separate always-on voltage domain with battery back-up. The RTC uses an[color=#f00] independent oscillator[/color], also located in the always-on voltage domain.


0 项奖励
回复

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mattiad on Mon Sep 08 14:22:01 MST 2014
Thank you,

so you can confirm me that the crystal is necessary? This is what I suppose.
0 项奖励
回复

2,654 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 08 13:39:05 MST 2014
Hardware: RTC Hardware is described in schematic of LPCXpresso LPC11U68:

http://www.embeddedartists.com/products/lpcxpresso/lpc11U68_xpr.php

Software: LPCOpen should include a RTC sample:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0
0 项奖励
回复