LPC11U35FHI33/501 USB HID ROM API NAK Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U35FHI33/501 USB HID ROM API NAK Issue

1,427 Views
BBQ
Contributor I

I am working on LPC11U35FHI33/501 as USB HID device using ROM API(USB on-chip driver).

< Issue >
HID Device send NAK to USB host when USB host send OUT transaction (Interrupt out) to device.
At first, ACK is returned normally, but at a certain point it becomes NAK, and after that NAK is returned always.

< Question >
What are the conditions under which a device returns a NAK?

Labels (3)
0 Kudos
Reply
1 Reply

1,369 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @BBQ 

Recommend you check the application code in USB device. This is depends on device application code.

 

BR

Alice

0 Kudos
Reply