LPC11C24 CAN Send test problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11C24 CAN Send test problem

1,140件の閲覧回数
funa
Contributor I

With OM13093.I took two wires in TXD and RXD, measured with an oscilloscope, and then run the following program. Found no signal. It  was found that VCC is always 0. Does VCC requires an  external power supply?

while(1) {
        msg_obj.msgobj  = 0;
        msg_obj.mode_id = 0x345;
        msg_obj.mask    = 0x0;
        msg_obj.dlc     = 4;
        msg_obj.data[0] = 'T';    // 0x54
        msg_obj.data[1] = 'E';    // 0x45
        msg_obj.data[2] = 'S';    // 0x53
        msg_obj.data[3] = 'T';    // 0x54
        LPC_CCAN_API->can_transmit(&msg_obj);
        for(j=0;j<1000000;j++) {
            ;
        }
        Board_LED_Toggle(0);
    }

0 件の賞賛
返信
1 返信

1,075件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

It is not normal that VCC=0v. It is not necessary additional supply for VCC.
 where are you doing this measurement? do you have additional connections?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信