LPC1114 indirect register access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1114 indirect register access

1,073 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wyorin on Thu Aug 14 07:50:55 MST 2014
This may be a dumb question, but I would like to set up pointers in Flash memory to the configuration registers for the I/O on an LPC1114 processor, e,g. registers of the form LPC_IOCON->PIO0_1. Is this possible.?
Labels (1)
0 Kudos
Reply
1 Reply

1,053 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Thu Aug 14 10:04:10 MST 2014
Hello,

The multiplexed pins most certainly can be structured to be user friendly and readable in the way you are mentioning. In fact, our software platform called LPCOpen provides software examples that structure things in this way, as well as easy API calls. Here's a link to the LPCOpen downloads:
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc11xx-packages-0

Even if your board is not supported, it would be helpful to look at the way things are declared. A quick glance at the UART example shows that the registers can be indirectly accessed like so: pIOCON->PIO0[pin].
0 Kudos
Reply