LPC1112 SOIC-20 availability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1112 SOIC-20 availability

1,147 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Thu Jul 31 06:47:38 MST 2014
Since nearly one year now, I'm trying to get a LPC1112 in SOIC-20 package, but no distributor has these parts. NEVER!!  |(
Kind of strange status 'production'. Disappointing.

I'm interested in this device, because I have designed a board for our company using LPC1110 and I'd like to use a LPC1112 while developing
the program (using execution from RAM). Also, having a bigger device available just in case the LPC1110 turns out to be too small would be a great option.

Does anyone own a few such a devices and would be so kind to sell me??

Marc



Labels (1)
0 Kudos
Reply
1 Reply

1,139 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Fri Aug 29 03:11:38 MST 2014
Thanks to forum member Rick's information, I got hold of 50 pieces of these from avnet USA :bigsmile:
...OK...for an really bad price, because of shipping costs  |(

One of these is already put to work and that eases my development - great!

If anyone in Europe has the same approach and problem like me, I'm willing to sell one
or two for that exact purpose.

Marc
0 Kudos
Reply