LPC1112 - hardfault on PDRUNCFG register write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1112 - hardfault on PDRUNCFG register write

2,104件の閲覧回数
danielkowalski
Contributor I

Hello,

I encountered strange problem with LPC1112 MCU when creating new design.

MCU mysteriously hard-faulted before reaching main, so I started debugging startup code (this works perfectly fine) and found problematic line in CMSIS source (system_LPC11xx.c):

LPC_SYSCON->PDRUNCFG &= ~(1 << 5); /* Power-up System Osc */

After reading through manual I found that some reserved bits need to be set to 1 in PDRUNCFG during write,

I tried setting register value to reset value (with required reserved bits), before even calling SystemInit.

Result is still the same - I get HardFault even with simple write to register:

LPC_SYSCON->PDRUNCFG = 0b1110110111110000;

The only thing happening before that is filling bss with zeros and copying data section to RAM.

what might be wrong with this? (I cannot configure system clock)

MCU is LPC1112FHI33/202.5

Daniel

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,954件の閲覧回数
Dezheng_Tang
NXP Employee
NXP Employee

Daniel,

    There is a possibilty that you used SYS OSC as the clock source for SYSPLLCLKSEL already and MAINCLK is derived from SYS OSC already, then you power down the SYS OSC in PDRUNCFG, you will get the hard fault.

If you use IRC as the clock source in SYSPLLCLK and MAINCLK, then, it will be OK to power down SYS OSC to lower the overall power consumption. Try this:

http://www.nxp.com/products/software-and-tools/hardware-development-tools/lpcxpresso-boards/lpcopen-...

0 件の賞賛
返信

1,953件の閲覧回数
danielkowalski
Contributor I

Hello,

I found the problem - Code was compiled for wrong core (facepalm).

I copied project from earlier revision, but I forgot that it used Cortex-m3 chip and LPC1112 is Cortex-M0.

Copynig data and zeroing BSS worked fine because it only used instructions supported by both cores, but when it came to writing registers

everything blew up.

Thanks for the help,

Daniel

0 件の賞賛
返信