LPC-link 2 + windows 10 driver problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-link 2 + windows 10 driver problems

3,600 Views
maker4433
Contributor I

I'm running Windows 10 in VirtualBox on Mac OSX.

With LPC Xpresso cannot connect to LPC link 2.

Looking in the Windows 10 "Devices and Printers" control panel there is a warning sign on the LPC Link 2 icon which leads to information as below.

All the drivers and sofware versions are the latest and have restarted.

Any suggestions please?

Device USB\VID_1FC9&PID_0090\JQD4FXOT had a problem starting.

Driver Name: usb.inf
Class Guid: {36fc9e60-c465-11cf-8056-444553540000}
Service: usbccgp
Lower Filters:
Upper Filters:
Problem: 0xA
Problem Status: 0xC000000D

(Windows 10 Screenshot attached too.)

0 Kudos
Reply
1 Reply

2,482 Views
lpcxpresso_supp
NXP Employee
NXP Employee

First of all, I assume that you know that LPCXpresso IDE with LPC-Link2 will work natively on Mac OS X ?

Its also worth saying that our own experience of VirtualBox on Mac OS X was not very positive, from the USB support side of things (though that was a while ago). Our Mac OSX users now generally use VMWare, and increasingly Parallels to run Windows on Macs.

But that aside, try going through : LPC-Link2 fails to enumerate with CMSIS-DAP firmware 

Its also possible that pre-programming the Link2 probe firmware rather than letting the IDE softload it might help : LPC-Link2 Debug Probe firmware programming 

Regards,

LPCXpresso Support

0 Kudos
Reply