LPC blhost utility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC blhost utility

Jump to solution
1,920 Views
DanielePagani
Contributor II

    Dear sirs,

we're using sdphost and blhost utilities for upgrading firmware of i.MX RT 1060 processor.

Now we're studying LPC822 and we're wondering if similar applications exist.

We found the basic commands in the document UM10800 - LPC82x User Manual and an external application (Flash Magic).

Is there something similar to blhost for the command line and cross-platform (Windows,Mac)?

BR

Daniele

Labels (1)
0 Kudos
Reply
1 Solution
1,803 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Daniele Pagani

for LPC82x, the recommended programmer is FlashMagic. User can program chip with on chip ISP mode.

Besides, we don't have other programmer (like blhost).


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,804 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Daniele Pagani

for LPC82x, the recommended programmer is FlashMagic. User can program chip with on chip ISP mode.

Besides, we don't have other programmer (like blhost).


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply