LPC1549 with screen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1549 with screen

1,593件の閲覧回数
maija_somero
Contributor I

Hi!

i’m using LPC1549 and am wondering if I can connect to it a Powrtip Pc1602 LCD screen. Where to find help with this?

ラベル(1)
0 件の賞賛
返信
1 返信

1,494件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Maija Somero,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
We do not have libraries for the implementation of the LCD 1602 with the LPC. However, I recommend you to see the following post in the community: Driving 1602 LCD using KSDK drivers
In the post, they use the FRDM-KL25Z card with the SDK drivers. You can use this example to see how they do all the configurations, initializations and sending data to the LCD. This way you can implement exactly the same drivers, only with the LPC drivers provided in the LPCOpen.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信