LPC blhost utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,856件の閲覧回数
DanielePagani
Contributor II

    Dear sirs,

we're using sdphost and blhost utilities for upgrading firmware of i.MX RT 1060 processor.

Now we're studying LPC822 and we're wondering if similar applications exist.

We found the basic commands in the document UM10800 - LPC82x User Manual and an external application (Flash Magic).

Is there something similar to blhost for the command line and cross-platform (Windows,Mac)?

BR

Daniele

ラベル(1)
0 件の賞賛
返信
1 解決策
1,739件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Daniele Pagani

for LPC82x, the recommended programmer is FlashMagic. User can program chip with on chip ISP mode.

Besides, we don't have other programmer (like blhost).


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,740件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Daniele Pagani

for LPC82x, the recommended programmer is FlashMagic. User can program chip with on chip ISP mode.

Besides, we don't have other programmer (like blhost).


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信