LPC-LinkII UART baud

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-LinkII UART baud

1,647 Views
JiaAn
Contributor I

Hi guys,

I am confused at LPC Link II UART baud.

I got an example code from LPC Open. There's an example code. It's named "periph_uart". I upload it to my board. And it seems can not work. Only receive garbled. I tried MB3232I and Arduino. Both of them received garbled.

But if I change the baud rate to 9600. (Example code is 115200) They can receive correctly. Does this means this board can only send UART with baud 9600? Or where should I check to speed up the baud rate?

Labels (2)
0 Kudos
Reply
1 Reply

1,636 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JiaAn

Which demo board do you work with? Could you send me a link of it? I will test it on my side.

Meanwhile, could you please also test other demos included in LPCOpen package?

How does it work on other computer?

Thanks,

Jun Zhang

0 Kudos
Reply