LPC-Link2 problem with CMSIS-DAP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC-Link2 problem with CMSIS-DAP

跳至解决方案
2,719 次查看
vlad23
Contributor I

Hello,
I have an LPC-Link2 board with a flashed CMSIS-DAP script, but when starting debugging with the openOCD, I get an error: "Error: CMSIS-DAP command CMD_INFO failed". What could be the problem? The computer correctly detects the LPC-Link2 in CMSIS-DAP mode. I also noticed that the chip LPC4370  heats up and the consumption of the board is 200mA at 3.3 volts, is this normal?

0 项奖励
回复
1 解答
2,664 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

在原帖中查看解决方案

3 回复数
2,684 次查看
vlad23
Contributor I

Hi @Miguel04 
Yes i get this error with any project. This problem arose from the unpacking of the LPC-Link2, it's always this error. I tried to connect a second LPC-Link2, this error does not occur on it and the debugger works.

0 项奖励
回复
2,665 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

2,690 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

I'm afraid it is not normal.

Do you have this problem everytime you run any project?

This happens only when you debug your project?

This could be the board is burned. 

Best Regards, Miguel.

0 项奖励
回复