LPC-Link2 problem with CMSIS-DAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 problem with CMSIS-DAP

ソリューションへジャンプ
2,849件の閲覧回数
vlad23
Contributor I

Hello,
I have an LPC-Link2 board with a flashed CMSIS-DAP script, but when starting debugging with the openOCD, I get an error: "Error: CMSIS-DAP command CMD_INFO failed". What could be the problem? The computer correctly detects the LPC-Link2 in CMSIS-DAP mode. I also noticed that the chip LPC4370  heats up and the consumption of the board is 200mA at 3.3 volts, is this normal?

0 件の賞賛
返信
1 解決策
2,794件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

元の投稿で解決策を見る

3 返答(返信)
2,814件の閲覧回数
vlad23
Contributor I

Hi @Miguel04 
Yes i get this error with any project. This problem arose from the unpacking of the LPC-Link2, it's always this error. I tried to connect a second LPC-Link2, this error does not occur on it and the debugger works.

0 件の賞賛
返信
2,794件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

2,820件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

I'm afraid it is not normal.

Do you have this problem everytime you run any project?

This happens only when you debug your project?

This could be the board is burned. 

Best Regards, Miguel.

0 件の賞賛
返信