LPC-Link2 problem with CMSIS-DAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 problem with CMSIS-DAP

Jump to solution
2,675 Views
vlad23
Contributor I

Hello,
I have an LPC-Link2 board with a flashed CMSIS-DAP script, but when starting debugging with the openOCD, I get an error: "Error: CMSIS-DAP command CMD_INFO failed". What could be the problem? The computer correctly detects the LPC-Link2 in CMSIS-DAP mode. I also noticed that the chip LPC4370  heats up and the consumption of the board is 200mA at 3.3 volts, is this normal?

0 Kudos
Reply
1 Solution
2,620 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

View solution in original post

3 Replies
2,640 Views
vlad23
Contributor I

Hi @Miguel04 
Yes i get this error with any project. This problem arose from the unpacking of the LPC-Link2, it's always this error. I tried to connect a second LPC-Link2, this error does not occur on it and the debugger works.

0 Kudos
Reply
2,621 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

If the problem started when you unpackage the board please contact with your distribuitor for the warranty.

I hope your issue gets a solution.

Best Regards, Miguel.

2,646 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @vlad23 

I'm afraid it is not normal.

Do you have this problem everytime you run any project?

This happens only when you debug your project?

This could be the board is burned. 

Best Regards, Miguel.

0 Kudos
Reply