LPC-Link2 board have support to flash program & debug for LPC5410X series MC ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 board have support to flash program & debug for LPC5410X series MC ?

2,077件の閲覧回数
ratheesht
Contributor II

Hi,

       I have the below LPC LINK2 development board.

         lpc-link-2.jpg

I have used this board to debug and flash the program for LPC11A04 MC.

Can i use this board to debug and flash for LPC5410X series micro-controller?

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

1,887件の閲覧回数
ratheesht
Contributor II

Thank you guys for immediate reply...

0 件の賞賛
返信

1,887件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Yes, you can use LPC-Link2 board in order to program & debug  LPC5410X series


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,887件の閲覧回数
converse
Senior Contributor V

Yes. Make sure you are using latest version of lpcxpresso.

0 件の賞賛
返信