LPC-Link2 board have support to flash program & debug for LPC5410X series MC ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 board have support to flash program & debug for LPC5410X series MC ?

2,096 Views
ratheesht
Contributor II

Hi,

       I have the below LPC LINK2 development board.

         lpc-link-2.jpg

I have used this board to debug and flash the program for LPC11A04 MC.

Can i use this board to debug and flash for LPC5410X series micro-controller?

Labels (5)
0 Kudos
Reply
3 Replies

1,906 Views
ratheesht
Contributor II

Thank you guys for immediate reply...

0 Kudos
Reply

1,906 Views
soledad
NXP Employee
NXP Employee

Hi,

Yes, you can use LPC-Link2 board in order to program & debug  LPC5410X series


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,906 Views
converse
Senior Contributor V

Yes. Make sure you are using latest version of lpcxpresso.

0 Kudos
Reply