LPC-Link2 : Is there a VCOM when using J-Link driver ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC-Link2 : Is there a VCOM when using J-Link driver ?

跳至解决方案
3,449 次查看
ybdecawave
Contributor I

Hi guys,

I am using the LPC-Link2 to debug a board under IAR ide. 

I have successfully been switching between CMSIS and J-link driver using LPCScrypt, but when using the J-link driver, I don't see any virtual com port associated to the board, only a J-link device. Is that expected ? 

In the NXP example below, it seems possible to have a virtual com port when using the LPC-Link2 as a J-link debugger (see 7:40 min)

Introduction to getting started with Amazon FreeRTOS and the LPC54018 IoT Module|NXP 

It is also specified on segger website :

LPCXpresso on-board | SEGGER - The Embedded Experts 

Thanks a lot,

Yves

0 项奖励
回复
1 解答
3,034 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Yves,

The firmware image for LPCXpresso V2 and V3 boards does include VCOM as of about a year ago. Make sure you are using the latest version of LPCScrypt to program your debug probe. The version for the standalone LPC-Link2 probe currently does not support this feature though.

I'll be talking to SEGGER about adding VCOM to LPC-Link2 ... the hardware does actually support it.

regards,

Brendon

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,035 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Hi Yves,

The firmware image for LPCXpresso V2 and V3 boards does include VCOM as of about a year ago. Make sure you are using the latest version of LPCScrypt to program your debug probe. The version for the standalone LPC-Link2 probe currently does not support this feature though.

I'll be talking to SEGGER about adding VCOM to LPC-Link2 ... the hardware does actually support it.

regards,

Brendon

0 项奖励
回复
3,034 次查看
ybdecawave
Contributor I

Hi guys,

For the record there is apparently not VCOM interface when using LPC-Link-2 with Jlink.

Jlink Segger Driver for LPC-Link2 nxp board : is virtual comport included ? - J-Link/Flasher related... 

Thanks

Yves

0 项奖励
回复