LPC Link 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Link 2

2,717 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tarakan on Tue May 10 00:03:55 MST 2016
Hi. I use LPC Link2 1 year as CMSIS DAP with Keil MDK. About a week ago MDK started with report RDDI-DAP error (MDK v5.18). (In MDK v5.15 report "SWD/JTAG Comunication Failure")
I tried:
a) New flash firmware to LPC Link2 with LPC Link 2 Configuration Tool
b) Second board LPC Link2
c) Remove and new instaling driver with lpc_driver_setup.exe
d) Instalink Keil MDK and everything another to second notebook
All with the same result. :-( Work on two projects with LPC824 stands.
Any idea?  Thank you.

Labels (1)
0 Kudos
Reply
5 Replies

2,368 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

2,368 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by allard_p on Tue May 10 11:08:55 MST 2016
Same problems here, i can debug/flash my LPC824 once. When i close the debugging session and start another i get a "invalid rom table" message. LPCxpresso can debug/flash the same LPC824 just fine. When i change my lpc-link2 to j-link firmware the LPC824 cant even be found.
0 Kudos
Reply

2,368 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue May 10 04:28:50 MST 2016
Have you tried this?
https://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
0 Kudos
Reply

2,368 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tarakan on Tue May 10 03:52:01 MST 2016
I bought a new LPC Link2. Therefore, I now have 2 pieces LPC Link 2. Reports the same error.
When I flash J-Link firmware to the LPC-Link2 MDK detect J-Link.
I cant through J-Link flash and debug Open1768 board (with LPC1768 MCU Cortex M3).
Unfortunately J-Link as SWD not detect LPC824 (Cortex M0) MCU.
0 Kudos
Reply

2,368 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue May 10 00:39:37 MST 2016
My guess is it is broken. Buy a new one.
0 Kudos
Reply