LPC Link 2 UART0 Access

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Link 2 UART0 Access

1,578 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoeE on Mon May 19 11:45:03 MST 2014
Hello all,
I am using the LPC LINK 2 as an evaluation board. So far, that works fine. Besides USART2 is it possible to get access to USART0 or USART3. I tried to configure the respective pins according to the Manual but that doesn't work. It seems that there is a problem with pin muxing, as activating pull up also does not work.
Thanks in advance
JoeE
标签 (1)
0 项奖励
回复
2 回复数

1,510 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoeE on Tue May 20 11:28:51 MST 2014
Thank you for the hint. UART0 works on that pins. UART3 still doesn't. But 2 UARTs is ok for me.
0 项奖励
回复

1,510 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Mon May 19 12:24:59 MST 2014
you can get the schematic here
http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php

UART0 on P6_4, P6_5
UART3 on P2_3, P2_4

however, the startup code probably already maps these pins to some other peripheral,
so you will have find where that code is, and disable that code before your code can enable the pins as a UART.
0 项奖励
回复