LPC 4357 10 bit A/D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 4357 10 bit A/D

1,264件の閲覧回数
peterweatherall
Contributor I

I see an intermittent problem with the LPC 4357 where the 10 bit AD converter does not flag the DONE bit after requesting a conversion under software control (START=1). This only happens in about 1 in 100000 measurements. In between each group of 4 measurements the converter is powered down. Is there any known issue that might cause this.

ラベル(1)
0 件の賞賛
返信
1 返信

1,201件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Peter Weatherall,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I'd like to get more information, such as code flow, testing steps,etc.
Whether you can share.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信