LPC 4357 10 bit A/D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 4357 10 bit A/D

1,321 Views
peterweatherall
Contributor I

I see an intermittent problem with the LPC 4357 where the 10 bit AD converter does not flag the DONE bit after requesting a conversion under software control (START=1). This only happens in about 1 in 100000 measurements. In between each group of 4 measurements the converter is powered down. Is there any known issue that might cause this.

Labels (1)
0 Kudos
Reply
1 Reply

1,258 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Peter Weatherall,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I'd like to get more information, such as code flow, testing steps,etc.
Whether you can share.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply