LPC 1837 & CAN - all messages

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1837 & CAN - all messages

1,266件の閲覧回数
phateee
Contributor II

Hello,

can me somebody help?LPC has only 32 can messages, which make interrupt.  It is posible to catch all messages on CAN?

I have: 

Init function

Chip_SCU_PinMuxSet(3, 1,(SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(3, 2,(SCU_MODE_INACT | SCU_MODE_FUNC2));


Chip_SCU_PinMuxSet(2, 13, (SCU_MODE_FUNC0 | SCU_PINIO_FAST));
Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT, 1, 13); /* GPIO5[6] = USB1_PWR_EN */
Chip_GPIO_SetPinState(LPC_GPIO_PORT, 1, 13, false); /* GPIO5[6] output high */

Chip_Clock_SetBaseClock(CLK_BASE_APB3, CLKIN_IDIVC, true, false);
Chip_CCAN_Init(LPC_C_CAN0);
Chip_CCAN_SetBitRate(LPC_C_CAN0, 500000);

Chip_CCAN_EnableTestMode(LPC_C_CAN0);
Chip_CCAN_ConfigTestMode(LPC_C_CAN0, (CCAN_TEST_BASIC_MODE | CCAN_TEST_BASIC_MODE));


Chip_CCAN_EnableInt(LPC_C_CAN0, (CCAN_CTRL_IE | CCAN_CTRL_SIE | CCAN_CTRL_EIE));

 NVIC_EnableIRQ(C_CAN0_IRQn);

and interrupt function:

void CAN0_IRQHandler(void)
{
CCAN_MSG_OBJ_T msg_buf;
uint32_t can_interrupt;
uint32_t can_status;
uint16_t can_mini_id_0 = 0;
uint16_t can_mini_id_1 = 0;
uint16_t i_mod = 0;

while ( (can_interrupt = Chip_CCAN_GetIntID(LPC_C_CAN0)) != 0 )
{
   if ((CCAN_INT_STATUS == can_interrupt) && (CCAN_STAT_RXOK & LPC_C_CAN0->STAT))
   {

      msg_buf.id = (LPC_C_CAN0->IF[CCAN_MSG_IF1].ARB1 | LPC_C_CAN0->IF[CCAN_MSG_IF1].ARB2 << 16);

      ..... 

       LPC_C_CAN0->STAT = LPC_C_CAN0->STAT & (~CCAN_STAT_RXOK);

    }

}

but I can't to catch any messages....

ラベル(1)
0 件の賞賛
返信
1 返信

1,144件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jan Mal&yacute

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
I'd already replied and please check the Case: 00125004
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信