LPC 1820 sometime will boot up fail !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 1820 sometime will boot up fail !

3,236 次查看
chenblake
Contributor I

Hello All: 

We got a boot up problem.

Our project use the LPC1820FBD144, the power source from USB VBUS.

I take USB cable plug in and plug out repeatedly.

Or press the reset button  repeatedly

It sometime will boot up fail.

The failure rate is 1~2  / 10 time. 

Is that  Known Issue?  

Because of I found the documents " LPC18XX-RN.pdf "

It mentions the similar problem.

" In a few hundred reset cycles one cycle might fail with a Hard Fault right after PLL initialization code "

If it is this known issue, how can we do?

If anyone meet the same problem.

or ,

If anyone has solution can resolve it.

Thanks

标签 (2)
0 项奖励
回复
5 回复数

2,777 次查看
chenblake
Contributor I

Hi Jeremyzhou:

Thanks for you reply.

I already found the cause.

That is NXP1820 PLL Clock frequency ramp-up need some delay for stable.

So, I add delay for it. And repair the problem.

The way is share for other user. See the bellow figure.

pastedImage_1.png

0 项奖励
回复

2,777 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Chen Blake,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

Before answer your question, I was wondering if you can tell me which boot mode you choose.
I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,777 次查看
chenblake
Contributor I

The boot mode is SPIFI.

0 项奖励
回复

2,777 次查看
converse
Senior Contributor V

There are some things in the errata that may be relevant 

http://www.nxp.com/documents/errata_sheet/ES_LPC18X0.pdf 

0 项奖励
回复

2,777 次查看
chenblake
Contributor I

Thanks for your reply and share!

0 项奖励
回复