LPC 1820 sometime will boot up fail !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1820 sometime will boot up fail !

4,863件の閲覧回数
chenblake
Contributor I

Hello All: 

We got a boot up problem.

Our project use the LPC1820FBD144, the power source from USB VBUS.

I take USB cable plug in and plug out repeatedly.

Or press the reset button  repeatedly

It sometime will boot up fail.

The failure rate is 1~2  / 10 time. 

Is that  Known Issue?  

Because of I found the documents " LPC18XX-RN.pdf "

It mentions the similar problem.

" In a few hundred reset cycles one cycle might fail with a Hard Fault right after PLL initialization code "

If it is this known issue, how can we do?

If anyone meet the same problem.

or ,

If anyone has solution can resolve it.

Thanks

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

4,404件の閲覧回数
chenblake
Contributor I

Hi Jeremyzhou:

Thanks for you reply.

I already found the cause.

That is NXP1820 PLL Clock frequency ramp-up need some delay for stable.

So, I add delay for it. And repair the problem.

The way is share for other user. See the bellow figure.

pastedImage_1.png

0 件の賞賛
返信

4,405件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Chen Blake,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

Before answer your question, I was wondering if you can tell me which boot mode you choose.
I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,404件の閲覧回数
chenblake
Contributor I

The boot mode is SPIFI.

0 件の賞賛
返信

4,404件の閲覧回数
converse
Senior Contributor V

There are some things in the errata that may be relevant 

http://www.nxp.com/documents/errata_sheet/ES_LPC18X0.pdf 

0 件の賞賛
返信

4,404件の閲覧回数
chenblake
Contributor I

Thanks for your reply and share!

0 件の賞賛
返信