LPC 1788 EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1788 EEPROM

1,643 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by peterd on Sat Jun 08 15:08:51 MST 2013

Is it possible to program the internal eeprom of the 1788 via ISP ?


It looks that the eeprom is not erased by a flash erase. So it is also not covered by the code protection.

Labels (1)
0 Kudos
Reply
2 Replies

1,545 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:41 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 Kudos
Reply

1,545 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:16 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 Kudos
Reply