LPC 1788 EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 1788 EEPROM

1,716 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by peterd on Sat Jun 08 15:08:51 MST 2013

Is it possible to program the internal eeprom of the 1788 via ISP ?


It looks that the eeprom is not erased by a flash erase. So it is also not covered by the code protection.

标签 (1)
0 项奖励
回复
2 回复数

1,618 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:41 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 项奖励
回复

1,618 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:16 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 项奖励
回复