LPC 1788 EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1788 EEPROM

1,640件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by peterd on Sat Jun 08 15:08:51 MST 2013

Is it possible to program the internal eeprom of the 1788 via ISP ?


It looks that the eeprom is not erased by a flash erase. So it is also not covered by the code protection.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,542件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:41 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 件の賞賛
返信

1,542件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Sat Jun 08 17:43:16 MST 2013

Going by the information in the LPC1788 user manual I would say not. By contrast, you can program the internal eeprom by IAP (not ISP) in the LPC1347 and that is specifically detailed in the LPC1347 user manual.

0 件の賞賛
返信