LPC 1768 CRP3 Enabled Device Recover

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1768 CRP3 Enabled Device Recover

1,090 Views
vijayg
Contributor I

Hi,

We are using LPC1768 with CRP3 is enabled in the code for security purpose.

But due to some FOTA issue our Application is got corrupted and not running.

We want to recover this Device's either JTAG or ISP Mode.

Since CRP3 is enabled , LPC1768 not allowing JTAG and ISP Mode.

Please any suggestion to Recover those Device's.

 

 

Tags (1)
0 Kudos
Reply
1 Reply

1,073 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @vijayg 

I don’t believe the device can be recovered because, at the CRP3 level, both ISP  pin and SWD  are disabled.

Be aware that there is no built-in recovery for designs once CRP Level 3 is enabled. The most simplistic way of implementing a custom recovery mechanism involves the “Re-Invoke ISP” IAP call.

888888888888.jpg

BR

Alice

 

0 Kudos
Reply