LP54608 ISP UART PROBLEM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LP54608 ISP UART PROBLEM

1,559 次查看
Boopathy_Rangaraj
Contributor II

Hi,

        I've a Custom Board with LPC54608. It was working fine. After changing the Osc Freq in Example Api's, the Controller suddenly went to Frozen state and there was no response in McuExpresso IDE. Then I tried to erase the flash banks in UART ISP mode using Flash Magic. It worked fine only once, again it went back to Frozen state. but now I couldn't able to program via ISP mode also.

what could be the issue..?? How can I enter ISP mode again..??

 

Thank you.

 

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,544 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Boopathy_Rangaraj 

If you can't erase Flash in ISP mode. please make sure if your SWD interface was well designed. Refer this article:
https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565

If no problem on SWD design. and we can't connect board in ISP, we need to consider if you enable ECRP by accident.
Please see this article I ever wrote:
https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC546xx-Understanding-ECRP/ta-p/1375263

The part is permanently disabled when
On-chip Image(s) are ruined
SWD access prohibited
ISP entries prohibited

 

Have a nice day,

Jun Zhang

0 项奖励
回复