LCDVDx pins Datamapping change possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCDVDx pins Datamapping change possible?

2,006 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GokhanZorbeyOzcan on Tue Nov 15 08:35:37 MST 2011
Hello All,
I will be using LPC3250 for a cu::stom board. That board will be able to drive several TFT-LCD panels. Both  16 bit 1:5:5:5 mode and  24 bit 8:8:8 mode will be used. For the purpose of having an easy hardware design, are there any ways to change the Data Mapping of LCD module to LCDVDx pins?
Best Regards
Gokhan Ozcan
Labels (1)
0 Kudos
Reply
1 Reply

1,922 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Magicoe.Niu on Thu Dec 06 19:58:31 MST 2012
Hi,

Seems LPC3250 LCDVx pins is quite easy to compatible 16bit and 24bit lcd data bus, using the highest 5bit is enough. Attached is pin map, fyi.

B.R.

Magicoe
0 Kudos
Reply