Keil's MCB1700 development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keil's MCB1700 development board

1,178件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Elianco_ES on Mon Nov 03 13:11:19 MST 2014
Hello fellow programmers,

I'd like to configure the LPCXpresso v7.4.0 compiler

to work with Keil's  MCB1700 development board  which hosts NXP LPC1768 micro.

So far I used Keil's microvision5 to compile and run the programs without any problems

And it worked fine, however the free version limit is 32KB.

I also used the MBED NXP development board  and it worked fine.

So I'm switching to LPCXpresso v7.4.0 compiler.

Thanks in advance for your response.

ラベル(1)
0 件の賞賛
返信
1 返信

1,145件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 03 21:32:23 MST 2014
So, what is your question? What are you struggling to do?
0 件の賞賛
返信