Keil components manager incomplete?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil components manager incomplete?

1,322 Views
kevinr11082005
Contributor I

I'm working on a project on lpc1768 that needs to run as a USB host; I've managed to get it to run as a device but there doesn't seem to be any USB host component available; I only need to connect to another device through a VirtualCOM port and read a byte stream. The components manager for one of the available samples (USB host keyboard) looks like:

host-sample-components.png

host-sample-components-1.png

host-sample-components-2.png

In my current project there seems to be no USB host component:

device-project-components.png

device-project-components-1.png

device-project-components-2.png

How can I import the USB host component?

Labels (1)
0 Kudos
Reply
1 Reply

1,285 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

 Hi

I'm not familiar with the Keil component, I would recommend you to contact the Keil Support team:

Keil Product Support 

As I know, we can find LPC1700 usb host demo code from here

MDK5 - Keil MCB1700 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply