Keil MDK5 for LPC4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil MDK5 for LPC4370

4,265 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Tue Jan 21 00:10:33 MST 2014
Hello friends,

Recently I downloaded mdk5 arm to use it for LPC4370 but I didn't find this controller in target option. Previous Keil mdk4.70 also doesn't have option for LPC4370. So is it possible to use keil for this controller? If it is possible, please let me know how do I do it. Any help regarding this will be highly appreciated.
Labels (1)
0 Kudos
Reply
7 Replies

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mburumaxwell on Sun Mar 01 09:21:49 MST 2015
You need to download the LPC4300 pack. When creating a new project select the right MCU. The LPC43xx family have a lot in common so they are put in the same pack. Here is a screenshot
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nmz787 on Wed Jan 22 13:39:58 MST 2014
I was able to get Keil MDK 5 lite talking to my LPC Link2 just by installing Keil, then flashing "CMSIS-DAP" firmware image with LPC Link2 Config-tool, then changing the debug/target config in Keil to use a CMSIS probe driver. Make sure to install JP1 after flashing CMSIS-DAP image!
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Tue Jan 21 03:59:15 MST 2014
Thank you very much TheFallGuy. I just missed that. Now I found the device listed in the target option after installing legacy support.
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 21 01:53:13 MST 2014
I just looked myself. Did you look here?

http://www2.keil.com/mdk5/legacy

It says:
- To use devices that are not yet supported by a Device Family Pack.
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 21 01:50:49 MST 2014
Why not ask on the Keil forums? They are the experts for their product.
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Tue Jan 21 01:23:21 MST 2014
Yes, I have look into their site, actually they have pack installer for installing desired family, but still they don't have option for lpc4370. I have look into internet, I think some have used Keil for this microcontroller, but I cannot find any option in it. So please help me regarding this.
0 Kudos
Reply

4,174 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 21 00:30:45 MST 2014
I think Keil changed how they deliver part support. IIRC, instead of delivering support files for every microcontroller that they support, you have to go to the Keil website and download the part support for the family you want.
0 Kudos
Reply