Jump to USB_Connect boot from code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jump to USB_Connect boot from code

Jump to solution
2,604 Views
jimc
Contributor I

OK This is probably impossible, but is there a way when running code, to jump to the rom bootloader and get it into USB Connect, to easily do an upgrade from the USB port?

Tags (1)
0 Kudos
Reply
1 Solution
2,571 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jimc 

It can jump to UART_ISP mode through "Reinvoke ISP":

Alice_Yang_0-1703495709902.png

 

BR

Alice

 

View solution in original post

0 Kudos
Reply
2 Replies
2,572 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jimc 

It can jump to UART_ISP mode through "Reinvoke ISP":

Alice_Yang_0-1703495709902.png

 

BR

Alice

 

0 Kudos
Reply
2,566 Views
jimc
Contributor I
THANKS!!!!!
0 Kudos
Reply