J-link "Error:Flash Download failed - Cortex-M0"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

J-link "Error:Flash Download failed - Cortex-M0"

4,443件の閲覧回数
katisr
Contributor I

Hello all,

I am using J-link seeger for debugging LPC43xx series using JTAG. I have just started programming with blinky ipc example.

When programming CM0,the program is built without errors, but unable to download to the board. The image of my error has been attached. 

Thanks in advance

タグ(2)
0 件の賞賛
返信
1 返信

3,709件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello katisr,

   What the code you are using?

  As I know, the official lpcopen multi core project, should build the M0 code at first, then build the M4 blink project, and download the M4 project, this project will call the according M0 function in the M4 code.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信