Is there any way that I can get the registerNotification work when board run the USB2Serial exaple plug & unplug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any way that I can get the registerNotification work when board run the USB2Serial exaple plug & unplug

675件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cgha on Sat Nov 24 02:28:17 MST 2012
I can only catch  DBT_DEVNODES_CHANGED event but no DBT_DEVICEARRIVAL and DBT_DEVICEREMOVECOMPLETE notification.
I use the microsoft msdn example to test it. But an commercial USB2SERIAL cable can get these event correctly.
So is there any other missing control packet that the example has not issued correctly?
Thanks!

ChrisChen

ラベル(1)
0 件の賞賛
返信
0 返答(返信)