Is there any tutorial on how to use LPC Link-2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any tutorial on how to use LPC Link-2?

3,079件の閲覧回数
vxs187
Contributor III

I am new to operating an LPC MC, would like to know if there is any shortcut route to using this, I am not an Embedded programmer, would like to know if there is any course that I might be able to do in order to get an insight on programming the MC and being able to use the same in a project. 

ラベル(1)
2 返答(返信)

2,589件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

I suggest you to check the following custom blog

https://mcu-things.com/blog/how-to-use-lpc-link2/ 

In addition please check the following videos:

LPC-Link 2 Debugger - YouTube 

LPC Tips & Tricks: LPCScrypt LPC-Link2 Debug Probe Programming - YouTube 

LPC-Link 2 Debug Adapter Extends LPCXpresso Ecosystem - YouTube 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,589件の閲覧回数
vxs187
Contributor III

Hi Sol,

I am using the UART TX to transmit messages to a computer through an Arduino, I guess the data rate of Link-2 is way higher than the data rate of the Arduino. I am not sure of it though, could you help me with this? 

0 件の賞賛
返信