Is it possible LPC1788 to support eMMC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible LPC1788 to support eMMC?

1,402件の閲覧回数
stefannikolov
Contributor I

Right now our device works with SD card, MMC card (almost) but eMMC is not working at all. We try with SanDisk and Samsung eMMC without luck.

ラベル(1)
0 件の賞賛
返信
1 返信

1,277件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Stefan,

According with the reference manual the LPC1788 supports SD card interface that also supports MMC cards only.
So, this devices does not support eMMC.


Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信