Is it possible LPC1788 to support eMMC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible LPC1788 to support eMMC?

1,460 Views
stefannikolov
Contributor I

Right now our device works with SD card, MMC card (almost) but eMMC is not working at all. We try with SanDisk and Samsung eMMC without luck.

Labels (1)
0 Kudos
Reply
1 Reply

1,335 Views
soledad
NXP Employee
NXP Employee

Hi Stefan,

According with the reference manual the LPC1788 supports SD card interface that also supports MMC cards only.
So, this devices does not support eMMC.


Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply