Is emWin full or basic version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is emWin full or basic version?

1,352件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eTrig on Mon Jan 14 00:50:54 MST 2013
Memdev or wm is not included basic version. What version is NXP provided?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eTrig on Mon Jan 14 01:26:19 MST 2013
Thanks for your relay.
0 件の賞賛
返信

1,340件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Mon Jan 14 01:03:26 MST 2013
Hi,

NXP provides the full version of emWin as compiled libraries. NXP has a license agreement with Segger, therefore the libraries are free to use (also for commercial purposes) on the NXP LPC microcontrollers. More information can be found at: http://www.lpcware.com/content/project/emwin-graphics-library

Regards,
Wouter
0 件の賞賛
返信