Is emWin full or basic version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is emWin full or basic version?

1,408 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eTrig on Mon Jan 14 00:50:54 MST 2013
Memdev or wm is not included basic version. What version is NXP provided?
Labels (1)
0 Kudos
Reply
2 Replies

1,396 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eTrig on Mon Jan 14 01:26:19 MST 2013
Thanks for your relay.
0 Kudos
Reply

1,396 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Mon Jan 14 01:03:26 MST 2013
Hi,

NXP provides the full version of emWin as compiled libraries. NXP has a license agreement with Segger, therefore the libraries are free to use (also for commercial purposes) on the NXP LPC microcontrollers. More information can be found at: http://www.lpcware.com/content/project/emwin-graphics-library

Regards,
Wouter
0 Kudos
Reply