Is LPC54608 simulator available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is LPC54608 simulator available

Jump to solution
1,898 Views
prathap_ponnuch
Contributor I

Hi,

I am using mcuxpresso IDE for LPC54608 code development.

There is some issue to get my ordered kit delay(COVID issue).IS there any possible to debug and verify code level development without hardware setup.

Thanks in advance.

regards,

prathap

Labels (1)
0 Kudos
Reply
1 Solution
1,848 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,849 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply