Is LPC54608 simulator available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is LPC54608 simulator available

ソリューションへジャンプ
1,905件の閲覧回数
prathap_ponnuch
Contributor I

Hi,

I am using mcuxpresso IDE for LPC54608 code development.

There is some issue to get my ordered kit delay(COVID issue).IS there any possible to debug and verify code level development without hardware setup.

Thanks in advance.

regards,

prathap

ラベル(1)
0 件の賞賛
返信
1 解決策
1,855件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,856件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信