Is LPC54608 simulator available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is LPC54608 simulator available

跳至解决方案
1,888 次查看
prathap_ponnuch
Contributor I

Hi,

I am using mcuxpresso IDE for LPC54608 code development.

There is some issue to get my ordered kit delay(COVID issue).IS there any possible to debug and verify code level development without hardware setup.

Thanks in advance.

regards,

prathap

标签 (1)
0 项奖励
回复
1 解答
1,838 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,839 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prathap,

As you know that the simulator is a feature of tools instead of hardware board, so it is dependent on the tools. Now, the LPC family supports MCUXpresso tools, Keil, IAR, I think none of them supports simulator without hardware board. BTW, in general only core simulation is supported even if simulator is supported.

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复