Inverter between LPC1769 and LAN8720 REFCLKO signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inverter between LPC1769 and LAN8720 REFCLKO signal

1,807 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marianoizzi@yahoo.com on Fri Feb 21 07:30:32 MST 2014
Hi guys,

I was wondering why there is an inverter (74LVC1G04GV) on the REFCLKO signal
between the LPC1769 and the LAN8720, on the LPCXpresso 1769 board.
Is it to delay the clock?

Labels (1)
0 Kudos
Reply
1 Reply

1,728 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by martinayotte on Sun Jan 18 14:39:32 MST 2015
I'm wondering getting such answer too, since most of the boards have one, but I have a board from Haoyu Electronics in China named LPC1768-MiniDK2 which doesn't have one, and the ethernet seems to work properly. Since I wish to design my own board, I don't know if it is really needed.
0 Kudos
Reply