Interrupt not serviced when using two capture pins on the same timer on LPC2132

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interrupt not serviced when using two capture pins on the same timer on LPC2132

892 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gvengineering on Mon Jan 11 15:03:04 MST 2016
Hello,

I have problems on my board trying to use two capture pins on the same timer.

My purpose is to use CAP0.2 (PIN0.28) and CAP0.3 (PIN0.29) on Timer0 in order to generate two interrupt.
CAP0.2 is set to generate an interrupt on a Rising Edge and CAP0.3 on a falling edge.

The problem is that if I use only CAP0.3 I have the Interrupt serviced and handled correctly, If I add also CAP0.2, no interrupts are handled.
In debug I can see the Interrupt request on the VIC peripheral but no call to ISR is done.

If I use only CAP0.2 again, no Interrupt is serviced even if the request is in the VIC

It seems only CAP0.3 it is working properly.

Here is the simple code I'm trying to run:



void __irq timers_isr0 ( void) 
{

if ( T0CR2 != StoreA )
{
StoreA = T0CR2;
countA++;
T0IR |= 0x40;
}

if ( T0CR3 != StoreB )
{
StoreB = T0CR3;
countB++;
T0IR |= 0x80;
}

T0TCR |= 0x02;//ResetCounter
T0TCR &= 0xFD;

VICVectAddr = 0x00;
} 

int main (void)
{

PINSEL0 = 0x00000000;
PINSEL1 = 0x0A000000;
// Enable Debug Port
PINSEL2 |= 0x00000034;
// Do Not Remove

// configure timer 0
T0CTCR = 0x08 ;  //   bit 00001000

T0TC   = 0;  /* Set Timer 0 Counter*/
T0PR   = 0;  /*  Set Prescaler */
T0CCR = 0x00000D40;

T0MCR = 0x00;
T0MR0 = 0x01;
T0MR1 = 0x00;
T0MR2 = 0x00;
T0MR3 = 0x00;
T0TCR = 0x01;  /* Start Timer*/

VICIntSelect = 0x00; /* */
VICVectCntl1 = 0x20 | 0x04; /* */
VICVectAddr1 = (unsigned) timers_isr0; /**/
VICIntEnable = 1 << 0x04; /* */

T0IR |= 0xFF;
while (1);

} // timers_init



THanks to anyone who could provide a suggestion.
Gabriele
标签 (1)
0 项奖励
回复
0 回复数