Issue with LP2364 UART communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with LP2364 UART communication

976件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NeethuG on Wed Oct 14 01:36:33 MST 2015
Dear All,

I am trying to implement UART0 communication in LPC2364.

I am using Sample Code Bundle for LPC23xx/LPC24xx Peripherals using Keil's μVision downloaded from the link 
https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-%C...

In start up code OSCEN is set but when we check the "System control and status" window, the register is found reset.

I am not able to set a desired baud rate also.

There is problem with interrupt also... Interrupt is getting fired but its not entering into start up code.


Please give your valuable suggestions

ラベル(1)
0 件の賞賛
返信
0 返答(返信)